CAN bus sniffer with MPC56xx?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN bus sniffer with MPC56xx?

跳至解决方案
1,621 次查看
borjagomez
Contributor I

Dear Sir/Madam:

 

I have to configure the FlexCAN module to work as a CAN bus sniffer or in normal mode (with msg Id related to a message buffer). I have no problem to run the FlexCAN module when Message Id are known and hence, they are linked to a message buffer, but I would like to know if this module can be configured for the reception of unknown message identifiers. In this case, the CAN module should work as a gateway. It just sends what it has received. Is this possible?

 

Thank you in advance,

 

Borja Gómez

标签 (1)
0 项奖励
回复
1 解答
1,483 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

You could just set a mask acceptance register(s) properly, means clear all bits. In that case the received ID is “don’t care”. If you want to receive both standard and extended frames then 2 MBs should be set for receive, one for standard and other for extended frames.

Regards,

Petr

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,484 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

You could just set a mask acceptance register(s) properly, means clear all bits. In that case the received ID is “don’t care”. If you want to receive both standard and extended frames then 2 MBs should be set for receive, one for standard and other for extended frames.

Regards,

Petr

0 项奖励
回复
1,483 次查看
borjagomez
Contributor I

Thank you very much.

Borja.

0 项奖励
回复