CAN FD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN FD

3,193件の閲覧回数
NVPR
Contributor I
  • Subject : CAN FD implementation
  • Description : We are using MPC 5744 P Dev Kit for one of our project haiving CAN FD requirement. We have connected the PEAK CAN simulator to CAN _0 port. Found that CAN FD is not working in the board. We have disabled the loopback in the FlexCAN example application and tested with the PEAK CAN simulator. We are using a bus speed of 500 kHz. Please provide the clock settings for this frequency. It is urgent and our project istalled now
0 件の賞賛
返信
5 返答(返信)

3,124件の閲覧回数
NVPR
Contributor I

Thanks. CAN extened ID is working. But is there any solution around MPC 5744P for CAN FD ?

0 件の賞賛
返信

3,111件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

unfortunately not, FlexCAN simply does not support CAN FD on MPC5744P, so there is no solution.

BR, Petr 

0 件の賞賛
返信

3,182件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

FlexCAN module on MPC5744P does not support CAN FD. 

BR, Petr

0 件の賞賛
返信

3,178件の閲覧回数
NVPR
Contributor I

OOH No, Actually  I require CAN FD.

Will it support normal CAN with extended ID ?

If it supports what are the clock settings for 500 KHz bit rate ?

0 件の賞賛
返信

3,173件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, normal CAN message with ext/std ID is supported.
For CAN bit timing calculation you can use below tool
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-S32Kxx-CAN-CAN-FD-bit-timing-calculation...

BR, Petr

0 件の賞賛
返信