Bootloader on MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader on MPC5777C

ソリューションへジャンプ
7,282件の閲覧回数
berat24
Contributor III

Hello everyone,

When I looked at the reference manuel for serial bootloader, I saw that eSCI baud rate should be 48000 for 40 MHz clock frequency.

However, rappid bootloader tool does not have any baud rate setting for 48000. Is there a different tool for sending our application code apart from rappid bootloader tool?

There are two different photos below, one of them is from reference manuel and another is from rappid bootloader tool.

Sincerely.

 

0 件の賞賛
返信
1 解決策
7,252件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

No, we have only Rappid bootloader. This bootloader used BAM for MPC56xx devices but then it was changed to flash resident bootloader in case of MPC57xx devices because the features have changed.

So, we don't have such tool, it needs to be developed by user.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
7,268件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

Rappid bootloader does not use Serial Boot mode on MPC5777C. In case of MPC57xx devices, Rappid bootloader is always flash resident bootloader, so it's necessary to load RBF file to the flash by JTAG. Then it's a matter of software configuration done by Rappid bootloader.

Regards,

Lukas

0 件の賞賛
返信
7,260件の閲覧回数
berat24
Contributor III

Hi,

I mean that I would like to use BAM module. However, I do not have any tool to send my application code. Is there any NXP tool in order to load my application code with BAM module.

Sincerely.

0 件の賞賛
返信
7,253件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

No, we have only Rappid bootloader. This bootloader used BAM for MPC56xx devices but then it was changed to flash resident bootloader in case of MPC57xx devices because the features have changed.

So, we don't have such tool, it needs to be developed by user.

Regards,

Lukas

0 件の賞賛
返信