It is possible to have more than one DCF record that writes to the same DCF client. DCF records are processed sequentially in the order they are read from flash memory. The later record overrides a DCF client value set by a previous record. Notice that not all DCF clients allow overwrites (UTEST Miscellaneous can be overwritten).
You can write the DCF records one by one until you reach the end of UTEST.
There’s also note:
“Be careful when programming the UTEST Miscellaneous,
XOSC ANA, and VREG Enable DCF clients. DCF records are
processed sequentially in the order they are read from flash
memory. DCF records that control actions such as enabling/
disabling voltage regulators or detectors should not be
programmed more than once with different values.”
Regards,
Lukas