Boot Application for MPC5775E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Application for MPC5775E

Jump to solution
2,962 Views
latheef
Contributor III

Hi All,

I am porting a Boot Application for MPC5775E from MPC5744P , so to start with I created a project using the S32DS to blink LED and I changed the default flash address from 00800000 to 0  in linker_flash.ld as below

/* Define FLASH */
/*FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ : 0x00800008;*/
FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ : 0x00000008;
/*FLASH_SIZE = DEFINED(__flash_size__) ? __flash_size__ : 2048K - 0x08;*/
FLASH_SIZE = DEFINED(__flash_size__) ? __flash_size__ : 128K - 0x08;

 

MEMORY
{
flash_rchw : org = 0x00000000, len = 0x4
cpu0_reset_vec : org = 0x00000000+0x04, len = 0x4

 

But when I try to flash with OpenSda I get the error during flash programming msg as  below

latheef_0-1666773229115.png

 

Log is shown as below

 

Connection from "127.0.0.1" via 127.0.0.1. Connection from port "63368" to 7224

Copyright 2018 P&E Microcomputer Systems,Inc.

Command Line :C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\pegdbserver_power_console -device=MPC5775E -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -speed=5000 -port=USB1¤

 

CMD>RE

 

Initializing.

 

Device IDCODE is $00000377

Device ID revision is $00000001

MPC5777C Device detected.

Target has been RESET and is active.

CMD>CM C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\gdi\P&E\nxp_mpc5775e_1x32x1024k_cflash_highspeed.pcp

 

Initializing.

 

Device IDCODE is $00000377

Device ID revision is $00000001

MPC5777C Device detected.

Initialized.

 

;version 1.00, 07/13/2018, Copyright P&E Microcomputer Systems, www.pemicro.com [5775EB_4meg_highspeed]

 

;device NXP, MPC5775E, 1x32x1024k, desc=CFlash_highspeed

 

;begin_cs device=$00800000, length=$00400000, ram=$00300000

 

Loading programming algorithm ...

Done.

Programming sequency is : erase, blank check, program, and verify {default}

CMD>VC

Verifying object file CRC-16 to device ranges ...

Error - no valid data in range of module.

Current content of flash does not match application to be programmed

CMD>EM

 

Erasing.

Module has been erased.

CMD>PM

 

Programming.

Processing Object File Data ...

                               

No data to program.

                               

.

Error during programming.

Error Programming flash of device

Error occured during Flash programming.

 

Device IDCODE is $00000377

Device ID revision is $00000001

 

Starting reset script (C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\gdi\P&E\s32e200_mpc5777c.mac) ... 

REM This script is compatible with MPC5777C devices.                                                                                                                                                     

REM Clean GPRs to remove residual data after using algorithm                                                                                                                                             

REM Setup MMU for for Periph B Modules                                                                                                                                                                  

REM Base address = $FFE0_0000                                                                                                                                                                           

REM TLB0, 2 MByte Memory Space, Guarded, Don't Cache, All Access                                                                                                                                        

Once Status Register Result = $0209

REM Set up MMU to put internal Flash at 0...                                                                                                                                                             

REM Virtual address 0x0 -> Physical address = $0000_0000                                                                                                                                                

REM TLB1, 16 MByte Memory Space, Not Guarded, Cachable, All Access                                                                                                                                      

Once Status Register Result = $0209

REM Set up MMU for External Memory                                                                                                                                                                       

REM Base address = $2000_0000                                                                                                                                                                            

REM TLB2, 16 MByte Memory Space, Not Guarded, Cachable, All Access                                                                                                                                       

Once Status Register Result = $0209

REM Set up MMU for Internal SRAM                                                                                                                                                                         

REM Base address = $4000_0000                                                                                                                                                                           

REM TLB3, 512 KByte Memory Space, Not Guarded, Don't Cache, All Access                                                                                                                                  

Once Status Register Result = $0209

REM Set up MMU for Periph A Modules                                                                                                                                                                      

REM Base address = $C3E0_0000                                                                                                                                                                            

REM TLB4, 2 MByte Memory Space, Guarded, Don't Cache, All Access                                                                                                                                         

Once Status Register Result = $0209

REM Initialize all of the Main SRAM - 512KB                                                                                                                                                             

Initializing RAM from $40000000 to $4007FFFF.

 

Reset script (C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.7.201906071634\win32\gdi\P&E\s32e200_mpc5777c.mac) completed.

 

MPC5777C Device detected.

PE-ERROR: Error downloading to the device.

Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "63368" from 7224

Target Disconnected.

 

Please let me know how to update the linker to properly flash to custom flash address?

Thanks,

Tags (1)
0 Kudos
Reply
1 Solution
2,948 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there are two pcp files from Pemicro:

lukaszadrapa_0-1666801137877.png

The first one (default one) covers only code flash starting at 0x800000.

The second one covers first blocks at 0x0 which are intended mainly for EEPROM.

If you want to program also this area, this configuration is necessary:

lukaszadrapa_1-1666801265218.png

Regards

Lukas

View solution in original post

3 Replies
2,949 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there are two pcp files from Pemicro:

lukaszadrapa_0-1666801137877.png

The first one (default one) covers only code flash starting at 0x800000.

The second one covers first blocks at 0x0 which are intended mainly for EEPROM.

If you want to program also this area, this configuration is necessary:

lukaszadrapa_1-1666801265218.png

Regards

Lukas

2,945 Views
latheef
Contributor III

Thanks for your reply @lukaszadrapa 

From your comment and reference manual the address 0 - 3FFFF is recommended for Data Flash and the boot is recommended to be in 800000 - 83FFFF. But since my boot won't go more than 32k, Is it OK to use the CSE (recommended) space for the boot application? 

latheef_0-1666814385558.png

Regards!

0 Kudos
Reply
2,932 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @latheef 

CSE blocks are dedicated to CSE only, those are not accessible by the main flash interface. So, this is not an option.

Regards,

Lukas