Basic MPC5676R question re; memory performance:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Basic MPC5676R question re; memory performance:

1,680 Views
laurentmeilleur
Contributor I

What is the performance of the on-chip FLASH and RAM?

 

2ns listing - tripped the Assumed answer flag, and couldn't reset to this still being an open question....

Labels (1)
0 Kudos
Reply
2 Replies

1,533 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

flash memory requires two wait states for read (RWSC parameter):

pastedImage_0.png

SRAM memory requires 1 wait state for system clock higher than 60MHz.

pastedImage_1.png

Then I would recommend this application note:

http://www.freescale.com/files/microcontrollers/doc/app_note/AN4324.pdf

http://www.freescale.com/files/microcontrollers/doc/app_note/AN4324_SW.zip

It shows how to optimize the settings to get maximum performance (enabling of cache, prefetch…).

Hope this helps.

Lukas

0 Kudos
Reply

1,533 Views
laurentmeilleur
Contributor I

Many thanks!

Laurent Meilleur

Vice President, Strategic Markets

DDC-I Inc.

220 River Reach Rd.

Swansboro, NC 28584

[email protected]

o: (602) 386-4343

m: (919) 619-6752

www.ddci.com

0 Kudos
Reply