BSP for MPC5644A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,615件の閲覧回数
janos_murai
Contributor III

Hi all,

I'm looking for a BSP for an MPC5644A processor, but I can't find any. It would also be good to find a BSP for a different processor, but with the same core (e200z4), so I could clone a new one.
I'd like to create an MQX based application. I work with an XPC56XX evaluation board.

 

I appreciate any relevant idea in this topic!

 

Thank you!

 

All the best,
Janos Murai

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,398件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

MPC56xx devices are not supported by our released MQX packages but you can contact http://embedded-access.com/  for help.

We provide Autosar/MCAL solutions for MPC56xx/57xx:

AUTOSAR™ Software|NXP 

Notice that it is commercial software.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,399件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

MPC56xx devices are not supported by our released MQX packages but you can contact http://embedded-access.com/  for help.

We provide Autosar/MCAL solutions for MPC56xx/57xx:

AUTOSAR™ Software|NXP 

Notice that it is commercial software.

Regards,

Lukas

0 件の賞賛
返信
2,398件の閲覧回数
janos_murai
Contributor III

Thank you Lukas, I'll contact them.

Best regards,

János Murai

0 件の賞賛
返信