Application code [MPC5744P]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Application code [MPC5744P]

1,067 次查看
abdelrhman
Contributor III

in MPC5744P, When I changed these memory addresses in the linker file,  the application did not start.  why did this behavior happen? 

from 0X00FA0000 
flash_rchw : org = 0x00FA0000, len = 0x4
cpu0_reset_vec : org = 0x00FA0000+0x04, len = 0x4

to 0X00FC0000
flash_rchw : org = 0x00FC0000, len = 0x4
cpu0_reset_vec : org = 0x00FC0000+0x04, len = 0x4



0 项奖励
回复
1 回复

1,062 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

When you setting the application boot is good to use bootable location as the SSCM module will scan only bootable locations for RCHW.

petervlna_0-1659606975008.png

Before going into such changes, I recommend you to get familiar with boot process.

Please refer to reference manual Chapter 55 Boot Assist Module (BAM)

Best regards,

Peter

 

0 项奖励
回复