Application code [MPC5744P]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Application code [MPC5744P]

1,062件の閲覧回数
abdelrhman
Contributor III

in MPC5744P, When I changed these memory addresses in the linker file,  the application did not start.  why did this behavior happen? 

from 0X00FA0000 
flash_rchw : org = 0x00FA0000, len = 0x4
cpu0_reset_vec : org = 0x00FA0000+0x04, len = 0x4

to 0X00FC0000
flash_rchw : org = 0x00FC0000, len = 0x4
cpu0_reset_vec : org = 0x00FC0000+0x04, len = 0x4



0 件の賞賛
返信
1 返信

1,057件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

When you setting the application boot is good to use bootable location as the SSCM module will scan only bootable locations for RCHW.

petervlna_0-1659606975008.png

Before going into such changes, I recommend you to get familiar with boot process.

Please refer to reference manual Chapter 55 Boot Assist Module (BAM)

Best regards,

Peter

 

0 件の賞賛
返信