About the MPC5634m eMIOS input capture and output compare

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About the MPC5634m eMIOS input capture and output compare

3,236 次查看
rongqin
Contributor II

Hi, Guys

I want to use the input caputure and output compare function in MPC5634m, but the code cannot realize the functions. Can you find the fault in my code? Thank you

//input capture

#include "MPC5634M_MLQC80.h"
unsigned int i=0;
unsigned int time1;
unsigned int time2;
unsigned int shuju[8];
void pll_init_80M(void)
{  
    FMPLL.SYNCR.R = 0x03080030;          /* Initial setting: 40 MHz for 8 MHz crystal */
    while (FMPLL.SYNSR.B.LOCK != 1) {};  /* Wait for LOCK = 1 */
    FMPLL.SYNCR.R = 0x03080430;            /* Enable FM */
    while (FMPLL.SYNSR.B.LOCK != 1) {};  /* Wait for FMPLL to LOCK again */  
    FMPLL.SYNCR.R = 0x03000430;            /* Final setting: 80 MHz for 8 MHz crystal */
}
void pll_init_64M(void)
{  
    FMPLL.SYNCR.R = 0x03080030;            /* Initial setting: 40 MHz for 8 MHz crystal */
    while (FMPLL.SYNSR.B.LOCK != 1) {};    /* Wait for LOCK = 1 */
    FMPLL.SYNCR.R = 0x03080430;            /* Enable FM */
    while (FMPLL.SYNSR.B.LOCK != 1) {};  /* Wait for FMPLL to LOCK again */  
    FMPLL.SYNCR.R = 0x16000000;         /* Final value for 64 MHz: RFD=0 */  
}
void initEMIOS(void)
{
  EMIOS.MCR.B.GPRE= 63;     /* Divide 64 MHz sysclk by 63+1 = 64 for 1MHz eMIOS clk*/
  EMIOS.MCR.B.ETB = 0;      /* External time base is disabled; Ch 23 drives ctr bus A */
  EMIOS.MCR.B.GPREN = 1; /* Enable eMIOS clock */
  EMIOS.MCR.B.GTBE = 1;  /* Enable global time base */
  EMIOS.MCR.B.FRZ = 0;
}
void initEMIOSch2(void)
{         /* EMIOS CH 9: Output Pulse Width Modulation */
  EMIOS.CH[2].CCR.B.BSL = 0x3;   /* Use internal counter */
  EMIOS.CH[2].CCR.B.FEN = 1;
  EMIOS.CH[2].CCR.B.EDSEL = 0;  /*Single edge triggering defined by the EDPOL bit*/  
  EMIOS.CH[2].CCR.B.EDPOL = 0;  /*Trigger on a falling edge*/
  EMIOS.CH[2].CCR.B.MODE = 0x02;  /* MPC551x, MPC563x: Mode is SAIC*/
  SIU.PCR[181].R = 0x0500;        /* Initialize pad for eMIOS chan. 2 output */
}
void EMIOS_RX_ISR(void)
{
    while(EMIOS.GFR.B.F2==0){    };
time1=time2;
time2=EMIOS.CH[2].CADR.R;
shuju[i] = time2-time1;
i++;
if(i>7)
i=0;

}
void main(void)
{
  
  pll_init_64M();
  initEMIOS();
  initEMIOSch2();
  INTC_InstallINTCInterruptHandler(EMIOS_RX_ISR,53,10);
  /* Loop forever */
  for (;;)
  {
     
  }
}

//output compare
#include "MPC5634M_MLQC80.h"
void pll_init_80M(void)
{  
    FMPLL.SYNCR.R = 0x03080030;          /* Initial setting: 40 MHz for 8 MHz crystal */
    while (FMPLL.SYNSR.B.LOCK != 1) {};  /* Wait for LOCK = 1 */
    FMPLL.SYNCR.R = 0x03080430;            /* Enable FM */
    while (FMPLL.SYNSR.B.LOCK != 1) {};  /* Wait for FMPLL to LOCK again */  
    FMPLL.SYNCR.R = 0x03000430;            /* Final setting: 80 MHz for 8 MHz crystal */
}
void pll_init_64M(void)
{  
    FMPLL.SYNCR.R = 0x03080030;            /* Initial setting: 40 MHz for 8 MHz crystal */
    while (FMPLL.SYNSR.B.LOCK != 1) {};    /* Wait for LOCK = 1 */
    FMPLL.SYNCR.R = 0x03080430;            /* Enable FM */
    while (FMPLL.SYNSR.B.LOCK != 1) {};  /* Wait for FMPLL to LOCK again */  
    FMPLL.SYNCR.R = 0x16000000;         /* Final value for 64 MHz: RFD=0 */  
}
void initEMIOS(void)
{
  EMIOS.MCR.B.GPRE= 63;     /* Divide 64 MHz sysclk by 63+1 = 64 for 1MHz eMIOS clk*/
  EMIOS.MCR.B.ETB = 0;      /* External time base is disabled; Ch 23 drives ctr bus A */
  EMIOS.MCR.B.GPREN = 1; /* Enable eMIOS clock */
  EMIOS.MCR.B.GTBE = 1;  /* Enable global time base */
  EMIOS.MCR.B.FRZ = 0;
}
void initEMIOSch2(void)
{         /* EMIOS CH 2: Output Pulse Width Modulation */
  EMIOS.CH[2].CADR.R = 100;      /*match value*/
  EMIOS.CH[2].CCR.B.BSL = 0x3;   /* Use internal counter */
  EMIOS.CH[2].CCR.B.EDSEL = 1;    /* the output flip-flop is toggled at each match*/
  EMIOS.CH[2].CCR.B.EDPOL = 1;   /* Polarity-leading edge sets output/trailing clears*/
  EMIOS.CH[2].CCR.B.MODE = 0x03;  /* MPC551x, MPC563x: Mode is SAOC */
  SIU.PCR[181].R = 0x0600;        /* Initialize pad for eMIOS chan. 2 output */
}
void initSIU(void)
{
   SIU.PCR[187].R = 0x0203;
}
int main(void) {
  volatile int i = 0;
  pll_init_64M();
  initEMIOS();
  initEMIOSch2();
  initSIU();
  /* Loop forever */
  for (;;)
  {
    SIU.GPDO[187].R = 0;
    if(EMIOS.CH[2].CADR.R == EMIOS.CH[2].CCNTR.R)
    {
      EMIOS.CH[0].CSR.B.FLAG =1;
      SIU.GPDO[187].R = 1;
    }
    if(EMIOS.CH[2].CADR.R == EMIOS.CH[2].CCNTR.R)
    EMIOS.CH[0].CSR.B.FLAG =1;
  }
}

0 项奖励
回复
5 回复数

2,121 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Channel 2 (medium channel) does not have internal counter, so cannot run from it.

pastedImage_1.png

So either select channel from the big group or select other counter bus for the channel 2 using CCR[BSL].

 

You can refer to the SAIC example in the following thread: https://community.nxp.com/message/605675

BR, Petr

2,121 次查看
翔宇童
Contributor I

but the emios[2] have SAIC(Single Action Input Capture)MODE ,this mode could return EMIOS_CADR[n]. But I cannot read the change of EMIOS_CADR[n]. How to exlplain it?

未命名1505188847.png

0 项奖励
回复

2,121 次查看
rongqin
Contributor II

Hi,

can you tell me that how to set the time for one count?

for eample 1count=1us

Thank you.

0 项奖励
回复

2,121 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi Rong,

the example I pointed to (https://community.nxp.com/message/605675) sets eMIOS global clock to 1MHz.

BR, Petr

0 项奖励
回复

2,121 次查看
rongqin
Contributor II

Thank you for your response, it is really helpful for me, Thank you.

0 项奖励
回复