About spc5777c external oscillator configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About spc5777c external oscillator configuration

跳至解决方案
2,291 次查看
liuxingqiao
Contributor I

Hello,

    According to the reference manual,  the on chip crystal oscillator can be bypassed to source a clock directly from the EXTAL pin(bypass mode),  and the bypass configuration is controlled by bit 24 of the Miscellaneous DCF record. I want to use an external oscillator to provide clock signal to EXTAL pin, and I have two questions:

  1. Should the XTAL pin be left unconnected, or be grounded?

  2. If bit 24 of the Miscellaneous DCF record is set to '1'(Oscillator enabled), would the external oscillator be influnced by internal oscillator circuits? Would the external oscillator or internal oscillator circuits be damaged?

Thanks.

0 项奖励
回复
1 解答
2,149 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) Leave XTAL pin floating.

2) No, it should not cause any damage. Disabling of internal oscillator in DCF client probably will lead in slightly decreased overall device power consumption.

在原帖中查看解决方案

2 回复数
2,150 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) Leave XTAL pin floating.

2) No, it should not cause any damage. Disabling of internal oscillator in DCF client probably will lead in slightly decreased overall device power consumption.

2,149 次查看
liuxingqiao
Contributor I

Thanks for your answer.

 

Best Regards,

 

liu xingqiao

0 项奖励
回复