Hi,everybody:
I have a question about cores for MPC5775K, I don`t know how to config these cores ,I want to use all of these cores so that I can get more performance, can you help me and give me a example about how to config core0 ,core1 and core2?
Thanks
Yanjun.Liang
已解决! 转到解答。
Hi,
you can find example codes here:
Only thing you must do is to add start of the cores as described in reference manual.
Here is example:
/*example code... need to be modified according to header file */
/* Enable Cores - Will start on next mode transition */
MC_ME.CCTL[2].R = 0x00FE; //z7a is enabled in all run modes
MC_ME.CCTL[3].R = 0x00FE; //z7b is enabled in all run modes
/* Set Start address for other cores: Will reset and start */
/* Flash addresses */
MC_ME.CADDR2.R = z7a_start_address; /* z7a */
MC_ME.CADDR3.R = z4b_start_address; /* z7b */
//Mode transition to apply the cores settings
MC_ME.MCTL.R = 0x30005AF0; //DRUN Mode & Key
MC_ME.MCTL.R = 0x3000A50F; //DRUN Mode & Key
while(MC_ME.GS.B.S_MTRANS); //Waiting for end of transaction
Peter
Hi,
you can find example codes here:
Only thing you must do is to add start of the cores as described in reference manual.
Here is example:
/*example code... need to be modified according to header file */
/* Enable Cores - Will start on next mode transition */
MC_ME.CCTL[2].R = 0x00FE; //z7a is enabled in all run modes
MC_ME.CCTL[3].R = 0x00FE; //z7b is enabled in all run modes
/* Set Start address for other cores: Will reset and start */
/* Flash addresses */
MC_ME.CADDR2.R = z7a_start_address; /* z7a */
MC_ME.CADDR3.R = z4b_start_address; /* z7b */
//Mode transition to apply the cores settings
MC_ME.MCTL.R = 0x30005AF0; //DRUN Mode & Key
MC_ME.MCTL.R = 0x3000A50F; //DRUN Mode & Key
while(MC_ME.GS.B.S_MTRANS); //Waiting for end of transaction
Peter
Hi,Peter
I have another question,what address I should set to the MC_ME.CADDR2.R or MC_ME.CADDR3.R?
I have seen the reference manual for MPC5775K,it saids that
But I don`t know about what value to set bit 0-29 and bit 31:
1. Field 0-29 said that means we can use 0-29 to set the boot address ,but I don`t know what specific value I should set.
2.Field 31 said that means whether we can reset Z4a by set 0 or 1 when the next mode changed,what does it mean by the next mode change? And what value do you usually set in field 31?
thanks
Yanjun.Liang
Hi,
1. I recommend you to always reset core on mode transition if you want to have it active after the mode transition.
2. Core Address - is really a start address for that particular core. So set it address when your code for that core starts.
Peter
Hi,Peter
As you said,I creat a new project ,it has 3 cores like this
1. I can`t find a definition whitch named "TURN_ON_CPU1 " and "TURN_ON_CPU2", when I define them ,it report that " warning: "TURN_ON_CPU1" redefined", so can you tell me where are they ?
2. I have transplant a demo code(MPC5775K-UART_with_Interrputs-S32DS_Z4_1), and it worked correctly in Z4 core.If I use this uart in Z4, Can I use the uart in Z7a and Z7b whithout configing this uart again? If I want to use some Buffs or defines in Z7,and these buffs was defined in Z4, How can I write my code?
3. The debug configrations
Does it mean that:
When I start the debug ,my project will start at Z4, and then Z7a and Z7b are both worked?
I have try to debug Z4 and set the break point in Z7a , but it can`t stop at Z7a break point ,how can I debug both Z4 and Z7?
One situation like that:
when I debug Z4 and set break point in Z7, my console remind that :there is no source in my file,and I have checked my file.
Why my debugger can`t find the file ? Should I set some specific config in "debug as"?
Please answer my questions ,thank you ~