Hello,
I am using 5674 MCAL for development.
But, when I am checking the test case Can_TC_0023, there is a confusing that:
1. Call Can_Init().
2. Verification Point: (Interrupt mode == CAN_INTERRUPT_DISABLED) &
(IntDisableLevel == 0)
3. Call Can_DisableControllerInterrupts() for 5 times.
4. Verification Point: (Interrupt mode == CAN_INTERRUPT_DISABLED) &
(IntDisableLevel == 5)
5. Call Can_EnableControllerInterrupts() for 4 times.
6. Verification Point: (Interrupt mode == CAN_INTERRUPT_DISABLED) &
(IntDisableLevel == 1)
7. Call Can_EnableControllerInterrupts() for one more times.
8. Verification Point: (0 == Can_ControllerStatuses[can_controller].
s8IntDisableLevel) & (Interrupt mode == CAN_INTERRUPT_ENABLED)
The first step, Can_Init() will set Interrupt mode to CAN_INTERRUPT_ENABLED.