AUTOSAR: What are software flags in CAN?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUTOSAR: What are software flags in CAN?

1,293 Views
Vasily_Wu
Contributor III

Hello,

I am using 5674 MCAL for development.

But, when I am checking the test case Can_TC_0024, there is a confusing that:

1. Call Can_Init().

2. Put controller into start state by calling Can_SetControllerMode().
3. Verification Point: (can_retval == CAN_OK)
4. Verification Point: (Check software flags)
5. Disable interrupt
6. Enable interrupt
7. Put controller into stopped state by calling Can_SetControllerMode().
8. Verification Point: (can_retval == CAN_OK) & software flag is cleared

What are software flags?

0 Kudos
Reply
1 Reply

1,264 Views
namnguyenviet
NXP Employee
NXP Employee

Since this is a legacy platform and the testing had been done in such a long time, unfortunately we don't know the answer.

Best Regards,

Nam

0 Kudos
Reply