A question about ADC Sampling time in MPC5643L.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A question about ADC Sampling time in MPC5643L.

ソリューションへジャンプ
1,459件の閲覧回数
jungwoojin
Contributor I

HI.

I use  MPC5643L.

this device includes two ADC modules, referred to as ADC_0, and ADC_1.

and it has 9 external channels each ( ex. ADC_0 channel0 ~ ADC_0 channel8)

I know I can set ADC sampling time for each ADC module.

Nevertheless, Can I set ADC sampling time differently for each external channel?

タグ(1)
0 件の賞賛
返信
1 解決策
1,364件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

more likely not. There is single CTR register for all external channels. So if you want to have different conversion time for each channel you need to reconfigure it before start of new channel conversion.

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,365件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

more likely not. There is single CTR register for all external channels. So if you want to have different conversion time for each channel you need to reconfigure it before start of new channel conversion.

BR, Petr

0 件の賞賛
返信
1,364件の閲覧回数
jungwoojin
Contributor I

Thanks for the reply.

I am using CTU to do all external channel's conversion automatically.

This is declared in the initialization phase as follows:

init.PNG

so, I wonder how i can reconfigure CTR register before start of new channel(The specific channel I want) conversion.

0 件の賞賛
返信
1,364件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

those 5 channels are converted immediately after each other, controlled by CTU. There is no way to change conversion time between each. You can maybe do that in SW controlled conversion.

BR, Petr

0 件の賞賛
返信