64-bit Global Variable Memory Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

64-bit Global Variable Memory Issue

5,009件の閲覧回数
ISLEMTRIKII
Contributor II

In my application, I needed to extend a global variable from 32 bits to 64 bits using MPC5644A.

unsigned long long extendedVar1 = 0x0ULL;

void function (unsigned long long var2 )

{

extendedVar1 |= var2;

}

The program builds every time, but sometimes it  fails to be flashed to the ecu, the flash memory is not fully used, but still this problem occurs when it's extended to 64 bits.

I tried an absolute addressing for this variable at the end of the flash and everything went well.

 

please find attached 2 screenshots from the memory allocations logs:

1- Problem has been solved with absolute memory allocation (mem.txt)

2- The same globale variable declared with no absolute memory allocation. (mem.txt)

 

Thank you!

0 件の賞賛
返信
3 返答(返信)

4,987件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you please specify used compiler?

0 件の賞賛
返信

4,982件の閲覧回数
ISLEMTRIKII
Contributor II

it's a : gcc (x86_64-posix-seh-rev0, Built by MinGW-W64 project) 8.1.0

  Thanks for your quick response!

0 件の賞賛
返信

4,915件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I see but it is not NXP software. It should discuss it is over particular provider's communities or other forums. Thanks for understanding

0 件の賞賛
返信