56xx SWT Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

56xx SWT Configuration

跳至解决方案
2,172 次查看
aero72
Contributor III

Can anyone suggest a reason as to what's wrong with this attempt to configure the SWT on a 56xx device.

On entry to the code SWT.CR.R = 0xFF00010A - so watchdog is disabled and SLK is cleared.

#define SWT_UNLOCK1      0xC520
#define SWT_UNLOCK2      0xD928
#define SWT_5MSTIMEOUT   0x13880     /* 16MHz Internal osc..@5ms timeout => 16MHz/200 = 80000 = 0x13880 */
#define SWT_SLK          0x00000010  /* Mask for software lock bit */
#define SWT_WEN          0x00000001  /* Mask for watchdog enable bit */

 /* Routine to setup software watchdog timer */
 /* If watchdog is disabled - set it up, otherwise leave it alone */
 if (!(SWT.CR.R & SWT_WEN))
 {  
    if (SWT.CR.R & SWT_SLK)
    {
     /* Soft lock bit is on - unlock the control register */
     /* Unlock the control register */
        SWT.SR.R = SWT_UNLOCK1;
        SWT.SR.R = SWT_UNLOCK2;
    }

    /*  Wait here for SLK to clear */
    while(SWT.CR.R & SWT_SLK);
   
    /* CR should now be writable  */
    SWT.CR.R |= SWT_WEN;
      
    /* Set timeout interval */
    SWT.TO.R = SWT_5MSTIMEOUT;
 }

On exit of this code, the SWT.TO register has been updated, but no matter what I do to write to SWT.CR (including, for instance SWT.CR.R = 0xFF00010B;) the watchdog remains disabled.

Any idea why this is?

Thanks for any suggestions.

标签 (1)
1 解答
1,984 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

This is because the debugger by default disable SWT.

Enable it in debug options of debugger or run your code wihtout debugger at all.

Peter

在原帖中查看解决方案

1 回复
1,985 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

This is because the debugger by default disable SWT.

Enable it in debug options of debugger or run your code wihtout debugger at all.

Peter