******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * start one Z7 core, interrupts initialization, ICache and DCache are disabled * on both cores because of shared memory, which must not be cached. * * There is 4K shared memory defined in the linker file. This memory is used by * both cores. Both cores access into the structure, which is placed in the shared * memory. This access is marked as a critical section. Only one core can write * to the structure at the same time. To ensure this, there are Gates, which * guarantee data coherence during the access. Only one core can be in critical * section. Second core has to wait, until first core leaves the critical section * * * * ------------------------------------------------------------------------------ * Test HW: MPC5775K-356DS, MPC57xx Motherboard * MCU: PPC5775KMMY3B 0N76P * Terminal: 19200-8-no parity-1 stop bit-no flow control on LINFlexD_0 * Fsys: PLL0 266MHz * Z4 Core 133MHz * Z7 Core 266MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: internal_FLASH (debug mode, release mode) * EVB connection: default connection * ********************************************************************************
記事全体を表示