Example S32R274 SWT_2 reset trigger GHS716

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example S32R274 SWT_2 reset trigger GHS716

Example S32R274 SWT_2 reset trigger GHS716

********************************************************************************
* Detailed Description:
* Test HW:  MPC57xx + S32R274RRUEVB
* Maskset:  1N58R
* Target :  internal_FLASH
* Fsys:     240 MHz PLL with 40 MHz crystal reference for z7 and 120MHz for z4
********************************************************************************
Revision History:
1.0     Apr-02-2019     b21190(Vlna Peter)  Initial Version
1.1    Apr-03-2019     b21190(Vlna Peter)  Added SWT reset reaction
*******************************************************************************/

This example demonstrated the reset trigger on first SWT_2 timeout.

Following screens shows the reset source after code execution in standalone mode and debugger connection afterwards:

pastedImage_1.png

pastedImage_2.png

添付
コメント

Hi Peter,

I am working on S32R274 and I need help for SWT_2.

I need your help regarding above code :

I am not able to see the NCFS_CFG0 is getting updated with my value 0x40000000 .

FCCU.NCFS_CFG[0].R = 0x40000000;.

and I can see that, NCF_S0  is showing value 0x00070000.

Below are the screen shot during debug :

SWT_2.PNG

Could please help me,. why this value NCF_S0 = 0x00070000, as I have just configure SWT_2 only.

and why I am not able to see the my written value in NCFS_CFG0.

Thanks !

Hi,

Hmm, and do you performing FCCU configuration in FCCU CONFIG mode?

regards,

Peter

Hi Peter, 

If timeout expires the SWT causes a reset, after this reset next timeout the SWT no longer reset.

I try the interrupt mode and the IR is correctly triggered in both cases but no reset after first reset.

What could be the problem?

What can I check?

Thank in advance.

Salvatore.

Hi petervlna

If timeout expires the SWT causes a reset, after this reset next timeout the SWT no longer reset.

I try the interrupt mode and the IR is correctly triggered in both cases but no reset after first reset.

What could be the problem?

What can I check?

Thank in advance.

Salvatore.

Hi,

Since you did not share much about your test setup, I guess it can be debugger whose preventing the code run or simply disable SWT as most debuggers do automatically.

regards,

Peter

Sorry, I've solved the problem. I had commented FCCU_clear_faults(). Now work.

Thanks

評価なし
バージョン履歴
最終更新日:
‎04-10-2019 03:02 AM
更新者: