Example MPC5748G SMPU initialization + Process ID test GHS614

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5748G SMPU initialization + Process ID test GHS614

Example MPC5748G SMPU initialization + Process ID test GHS614

********************************************************************************
* Detailed Description:
* This example initializes SMPU_0 and SMPU_1 to cover all memory resources for
* all masters.
* Simple test is performed in this example: after initialization, SMPU_1
* configuration is changed to disable write access to last 4kB of RAM for
* Process ID 1. Write acess is allowed for Process ID 0.
* If this area is written by CPU while the Process ID is 1, exception will
* occur due to access violation.
* ------------------------------------------------------------------------------
* Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C
* MCU:             PPC5748GMMN6A 1N81M
* Fsys:            160 MHz PLL
* Debugger:        Lauterbach Trace32
* Target:          internal_FLASH
*
********************************************************************************

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎09-07-2016 04:26 AM
更新者: