Example MPC5748G FlexCAN FD TX/RX S32DS2.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5748G FlexCAN FD TX/RX S32DS2.1

Example MPC5748G FlexCAN FD TX/RX S32DS2.1

********************************************************************************
 Detailed Description:

 Configures the FlexCAN_0 to transmit and receive a CAN FD message with or without
 bit rate switching for data phase.
 Baudrate during arbitration phase is set to 500kbps, during data phase 2Mpbs.

 NOTE! Termination resistor (120Ohm) have to be placed on transceivers output

 ------------------------------------------------------------------------------
 Test HW: DEVKIT-MPC5748G revD1
 Maskset: 0N78S
 Target : FLASH
 Fsys: 160 MHz PLL

********************************************************************************
Revision History:
1.0 Jun-21-2021 Petr Stancik Initial Version

*******************************************************************************/

添付
評価なし
バージョン履歴
最終更新日:
‎06-23-2021 05:09 AM
更新者: