Example MPC5748G Flash RW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5748G Flash RW

Example MPC5748G Flash RW

********************************************************************************

* Detailed Description:

*

* Unlock, erase and program of flash mid block 0x00FB_8000 - 0x00FB_FFFF.

* ------------------------------------------------------------------------------

* Test HW:        X - PC5748G - MB (rev C)

* MCU:             PPC5748GMMN6A

* Maskset:       1N81M

* Fsys:             160 MHz

* Debugger:     Lauterbach Trace32

*            

* Target:     Internal_FLASH

*

********************************************************************************

ラベル(1)
添付
コメント

Lukas,

In the "MPC5748G-Flash_RW-GHS614\source\main.c" file I see the bit settings for LOCK/SEL for Flash blocks on MPC5748G.

Shouldn't the Large blocks be using SEL2 instead of SEL0 ?

pastedImage_2.png

thanks

Anoop

Hi Anoop,

thanks for your comment. You are right, that's copy-paste issue. I uploaded corrected version.

Regards,

Lukas

t32_diff.png

Is it right?

Hi Lukas Zadrapa !!!

   Where can I download  Green Hills MULTI IDE v6.1.4 ? Think you!!!

評価なし
バージョン履歴
最終更新日:
‎06-03-2015 06:03 AM
更新者: