Example MPC5744P eTimer ADC injected conversion S32DS_2.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5744P eTimer ADC injected conversion S32DS_2.1

Example MPC5744P eTimer ADC injected conversion S32DS_2.1

********************************************************************************
 Detailed Description:

 This example shows ADC triggering from the eTimer1 module.
 The OFLAG signal from the eTimer1 channel 5 is fed into ADC1 converter,
 so ADC is set up for injected conversion with end of scan interrupt.

 Red LED is dimmed based on converted value

 ------------------------------------------------------------------------------
 Test HW: DEVKIT-MPC5744P rev.B
 Maskset: 1N16P
 Target : FLASH
 Fsys: 160 MHz PLL
 Debugger: S32DS

********************************************************************************

Attachments
No ratings
Version history
Last update:
‎04-23-2021 12:10 AM
Updated by: