Example MPC5744P FlexCAN simpleTXRX GHS614

cancel
Showing results for 
Search instead for 
Did you mean: 

Example MPC5744P FlexCAN simpleTXRX GHS614

No ratings

Example MPC5744P FlexCAN simpleTXRX GHS614

********************************************************************************

* Detailed Description:

*

*

* Initializes the MCU including the FlexCAN peripherals.

* Configures the FlexCAN to transmit and receive a CAN message.

*

* In this config, CAN_0 transmits a message. CAN_1 receives the message.

* CAN_0 MB8 is configured to send data. CAN_0 sends message each 1sec.

* This interval is generated by PIT.

* CAN_1 MB9 is configured to receive a message, SW polling is used.

*

* to connect FlexCAN0 module (MCU's PB0/PB1 pins) to the motherboard's transceiver

* with J5 CAN DB9 connector you have to:

* - connect J17 2-6 on daughter board

* - connect J17 5-3 on daughter board

* This should be done as default

 

* To connect FlexCAN1 module (MCU's PA14/PA15 pins) to the motherboard's transceiver

* with J6 CAN DB9 connector you have to:

* - connect J37 2-3 on motherboard

* - connect J38 2-3 on motherboard

*

* Connect CAN0-CANH on P15-1 to CAN1-CANH on P14-1

* Connect CAN0-CANL on P15-2 to CAN1-CANL on P14-2

* Terminate the CAN bus by connecting a 60 ohm resistor between CANH and CANL

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx

* Maskset:  1N65H

* Target :  internal_FLASH

* Fsys:     200 MHz PLL with 40 MHz crystal reference

*

********************************************************************************

Labels (1)
Attachments
Comments

Dear Diana Torres & Petr Stanc

Do you have SPC5744P's CAN transceiver software based on the S32DS for power V1.2 development environment demo?.

Hi everyone,

I am looking for an example of two  MPC5744P boards that communicate together using  FlexCAN protocol.

May someone help me?

Version history
Last update:
‎03-18-2015 12:56 AM
Updated by: