Detailed Description:
Initializes the MCU including the FlexCAN peripherals.
Configures the FlexCAN to transmit and receive a CAN message.
In this config, CAN_0 transmits a message. CAN_1 receives the message.
CAN_0 MB8 is configured to send data each 1sec.This interval is generated by PIT.
CAN_1 RXFIFO is configured to receive a message and interrupt for MB5 is enabled.
To connect FlexCAN0 module (MCU's PB0/PB1 pins) to the motherboard's transceiver
with J5 CAN DB9 connector you have to:
- connect J17 2-6 on daughter board
- connect J17 5-3 on daughter board
This should be done as default
To connect FlexCAN1 module (MCU's PA14/PA15 pins) to the motherboard's transceiver
with J6 CAN DB9 connector you have to:
- connect J37 2-3 on motherboard
- connect J38 2-3 on motherboard
Connect CAN0-CANH on P15-1 to CAN1-CANH on P14-1
Connect CAN0-CANL on P15-2 to CAN1-CANL on P14-2
Terminate the CAN bus by connecting a 60 ohm resistor between CANH and CANL
To see LED toggling connect P8.1 to USER LED (P7.x)
------------------------------------------------------------------------------
Test HW: MPC5744P EVB
Maskset: 1N65H
Target : RAM, internal_FLASH
Fsys: 200 MHz PLL with 40 MHz crystal reference