Example MPC5744P DMA multiple minor transfers GHS614

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5744P DMA multiple minor transfers GHS614

Example MPC5744P DMA multiple minor transfers GHS614

********************************************************************************

* Detailed Description:

* This example shows how to use eDMA for transfering 32-bit data multiple time using minor loop from internal flash to SRAM memory as well as how to configure AIPS (peripheral bridge) to grant eDMA access to peripherals.

*

* For closer details on how eDMA works I suggest you to check reference manual as this module is quite complex.

* This example sets system clock for 200MHz running from PLL0 module.

* The constant stored in internal flash is transfered via eDMA to SRAM memory.

* Initialization functions are AIPS_0_Init for peripheral bridge and DMA_0_Init.

*

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx Motherboard + MPC5744PE257DC minimodule, MPC5744P,

* silicon mask set 0N15P

* Target :  internal_FLASH*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎12-07-2015 07:21 AM
更新人: