Example MPC5675K Data_flash_program_simple CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5675K Data_flash_program_simple CW210

Example MPC5675K Data_flash_program_simple CW210

********************************************************************************

* Detailed Description:

* Example show simple flash programming routine. During runtime it changes

* content of field of constants 'test' (located in internal data flash).

* Also it shows how to relocate data into FLASH (used linker command file

* is MPC5675K_my_sections.lcf and MPC5675K_DEBUG_my_sections.lcf).

*

* Note: For complex tasks use SSD driver (Freescale site for particular device,

* Software&Tools/Run-Time Software/Middleware-Device Drivers

* ------------------------------------------------------------------------------

* Test HW:        MPC5675KEVB

* MCU:            PPC5675KFMMSJ in Lock-Step mode

* Fsys:           180/150 MHz CORE_CLK

* Debugger:       Lauterbach Trace32

*                 PeMicro USB-ML-PPCNEXUS

* Target:         RAM, internal_FLASH

* Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A

* EVB connection: default

********************************************************************************

标签 (1)
附件
100% 有帮助 (1/1)
版本历史
最后更新:
‎12-17-2015 06:27 AM
更新人: