Example MPC5643L Flash_program_simple CW210

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5643L Flash_program_simple CW210

Example MPC5643L Flash_program_simple CW210

********************************************************************************

* Detailed Description:

* Example show simple flash programming routine. During runtime it changes

* content of field of constants 'test' (thus located in internal flash).

* Also it shows how to relocate code into RAM a data into FLASH (used linker

* command file is MPC5643L_my_sections.lcf and MPC5643L_DEBUG_my_sections.lcf).

*

* Note: For complex tasks use SSD driver (Freescale site for particular device,

* Software&Tools/Run-Time Software/Middleware-Device Drivers

*

* ------------------------------------------------------------------------------

* Test HW:         xPC564xLKIT, PPC5643L Cut3 silicon

* Target :         internal_FLASH, RAM

* Fsys:            120 MHz PLL0

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0

* EVB connection:  default

*

********************************************************************************

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎08-11-2014 07:38 AM
更新者: