Example MPC5607B PinToggleStationery CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5607B PinToggleStationery CW210

Example MPC5607B PinToggleStationery CW210

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt,

* initializes and display notice via UART terminal and then terminal ECHO.

* ------------------------------------------------------------------------------

* Test HW:        XPC5607B 176LQFP, XPC56XX EVB MOTHEBOARD Rev.C

* MCU:             PPC5607BMLUAM03Y

* Fsys:             64/48 MHz

* Debugger:      Lauterbach Trace32

*                      PeMicro USB-ML-PPCNEXUS

* Target:           RAM, internal_FLASH

* Terminal:       19200-8-no parity-1 stop bit-no flow control on LINFLEX_0

* EVB connection: default

*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎12-17-2015 04:35 AM
更新人: