Example MPC5607B CAN sampler and STOP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5607B CAN sampler and STOP mode

Example MPC5607B CAN sampler and STOP mode

********************************************************************************

* Detailed Description:

* This example shows how to configure Wake up unit and CAN sampler.

* Once the device is woken up from STOP mode by falling edge on CAN0RX pin,

* the CAN sampler starts to sample this pin in given period.

* FlexCAN module is not initialized and used in this example because the CAN

* sampler is independent of FlexCAN.

* ------------------------------------------------------------------------------

* Test HW:  XPC56xxMB2 + XPC560B 176LQFP, PPC5607B

* Target :  internal_FLASH, RAM

* Fsys:     64 MHz PLL

*

********************************************************************************

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎03-24-2014 04:33 AM
更新者: