Example MPC5554EVB PinToggleStationery CW210

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5554EVB PinToggleStationery CW210

Example MPC5554EVB PinToggleStationery CW210

********************************************************************************
* Detailed Description:
* Application performs basic initialization, setup PLL to maximum allowed freq.,
* initializes interrupts, blinking one LED by interrupt, second LED by software
* loop, initializes and display notice via UART terminal and then terminal ECHO.
* The example configures the device for maximum performance (OPTIMIZATIONS_ON).
*
* ------------------------------------------------------------------------------
* Test HW:        MPC5554EVB
* MCU:            MPC5554MVR132
* Fsys:           132/112/80/12 MHz
* Debugger:       Lauterbach Trace32
*                 PeMicro USB-ML-PPCNEXUS
* Target:         RAM, internal_FLASH
* Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A
* EVB connection: TPU_PORT_37 -> USER_LED_8
*                 TPU_PORT_38 -> USER_LED_7 (to see blinking LEDs)  
*
********************************************************************************
Attachments
100% helpful (2/2)
Version history
Last update:
‎11-16-2022 07:26 AM
Updated by: