Example MPC5554 eQADC+INTC Single Scan CW210

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5554 eQADC+INTC Single Scan CW210

Example MPC5554 eQADC+INTC Single Scan CW210

********************************************************************************
* Detailed Description:
* Initializes eQADC module, performs calibration and converts channel 0 and
* displays results into terminal window by interrupt service routine. Analog
* input AN[0] requires external connection to converted voltage (potentiometer).
* ------------------------------------------------------------------------------
* Test HW:        MPC5554EVB
* MCU:            MPC5554MVR132
* Fsys:           132/112/80/12 MHz
* Debugger:       Lauterbach Trace32
*                 PeMicro USB-ML-PPCNEXUS
* Target:         RAM, internal_FLASH
* Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A
* EVB connection: USER_DEV pin RV2(i.e. pin8) -> pin B7 on I/O header ring
*                 (potentiometer RV2 to analog input AN[0])  
*
********************************************************************************
添付
コメント

very good,thank you

Hello, I burned the program in this example into MPC5554evb, but I don’t know how to verify it. How can I test and verify this example on MPC5554evb?

評価なし
バージョン履歴
最終更新日:
‎11-16-2022 07:27 AM
更新者: