simple pwm with FlexPWM0 MCXA153

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

simple pwm with FlexPWM0 MCXA153

ソリューションへジャンプ
854件の閲覧回数
berndgrossmann
Contributor II

I try to get a 1kHz PWM Signal on Pin 3.1 (45) of FRDM-MCXA153 board.

Peripheral is set to FlexPWM0 B,0 Pin to 45 Output

berndgrossmann_5-1732527655231.png

 

FlexPWM0 settings are

berndgrossmann_6-1732527655240.png

 

berndgrossmann_7-1732527655246.png

 

I try to get a controlled pwm Signal on pin 3.1 with on/off an duty cycle control.

Can someone help me?

0 件の賞賛
返信
1 解決策
821件の閲覧回数
Pablo_Ramos
NXP Employee
NXP Employee

Hi @berndgrossmann,
You can take as reference the pwm example of FRDM-MCXA153 SDK.

Pablo_Ramos_0-1732558596331.png

In order to have a better understanding about the example you can take a look to the readme file. In there you will find and overview, hardware requirements, board setting and how to prepare the demo.

Hope it helps you!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
822件の閲覧回数
Pablo_Ramos
NXP Employee
NXP Employee

Hi @berndgrossmann,
You can take as reference the pwm example of FRDM-MCXA153 SDK.

Pablo_Ramos_0-1732558596331.png

In order to have a better understanding about the example you can take a look to the readme file. In there you will find and overview, hardware requirements, board setting and how to prepare the demo.

Hope it helps you!

0 件の賞賛
返信