rt1186 debug issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rt1186 debug issues

630 Views
yanyanwang
Contributor I

After enabling OEM_CLOSE on the FRDM-IMXRT1186 development board, I can no longer debug the device. I saw in the reference manual that nxpdebugmbox can be used to re-enable debugging, but I tried it and was not successful.

yanyanwang_0-1788347257012.png

 

0 Kudos
Reply
4 Replies

617 Views
marek-trmac
NXP Employee
NXP Employee

Hello @yanyanwang 

In SEC tool documentation, you can find troubleshooting for debug authentication:

https://docs.mcuxpresso.nxp.com/secure/latest/09_troubleshooting.html#debug-authentication

Some useful tips can be also found in 

https://docs.mcuxpresso.nxp.com/secure/latest/07_generic_workflows.html#debug-authentication-workflo...

If this does not help, can you provide details about configuration? Could you share the SEC tool workspace settings?

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply

579 Views
yanyanwang
Contributor I

I have reviewed the links you provided and followed the recommended procedure, but I am still experiencing the same issue.

I only signed the image and did not encrypt it. I also set OEM_CLOSE.

I am using nxpdebugmbox only to re-enable the debug functionality.

I have uploaded the SEC project as an attachment, along with the relevant logs. Could you please help analyze the project and logs and identify the cause of the issue?

0 Kudos
Reply

562 Views
marek-trmac
NXP Employee
NXP Employee

@yanyanwang 

It seems this problem is related to SEC 26.03. We recommend updating to SEC 26.06. 

We are sorry for inconvenience.

Note: SEC 26.06 also contains fix for the SPARSE image format

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply

414 Views
yanyanwang
Contributor I
Yes, thank you. The authentication was successful, but I still cannot debug the device.

The procedure is as follows:

1. Use the SEC tool to perform the authentication.
2. The authentication is successful.
3. Then click the Debug button to start debugging.
4. However, the debugging attempt fails.

0 Kudos
Reply