iRTC failed to initialized using 32k osc on MCXN947

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iRTC failed to initialized using 32k osc on MCXN947

Jump to solution
3,490 Views
jimmyli
Contributor V

Hi NXP,

      I need to use outside 32K oscillator for iRTC in MCXN947.

      When I used MCUXpresso IDE to config and initialize the iRTC peripheral, it will fail when initialize clock source for iRTC.

      Hope you can check and provide a help to resolve this problem.

      Thanks very much.

 

 

1>MCUXpresso IDE config for iRTC

jimmyli_0-1765529502329.png

jimmyli_1-1765529532869.png

jimmyli_2-1765529589609.png

2>initial and hang here

jimmyli_3-1765529713752.png

 

 

 

Labels (1)
0 Kudos
Reply
1 Solution
3,378 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have been able to reproduce the error you have reported. The issue is caused by invalid configuration of the FRO16K of the VBAT. The FRO16K must be enabled and the outputs to VBAT and MAIN domain enabled. See the following screenshot:

marek_neuzil_0-1765810802158.png

This dependency on the FRO16K is not clearly stated in the reference manuals of the MCXN947 MCU. I will ask the responsible team for clarification of the correct initialization sequence for the the RTCCLKSEL clock selector that is a part of the RTC subsystem. The FRO16K must be enable to access the RTC subsystem register. We will also provide the fix for the MCXN947 MCU in the Clock tool to provide correct initialization code and dependencies in the Clocks model UI.

In the mean time, use the workaround specified above to use 32kHz crystal oscillator clock source as the LP_OSC clock source.

Best Regards,

Marek Neuzil

View solution in original post

9 Replies
3,379 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have been able to reproduce the error you have reported. The issue is caused by invalid configuration of the FRO16K of the VBAT. The FRO16K must be enabled and the outputs to VBAT and MAIN domain enabled. See the following screenshot:

marek_neuzil_0-1765810802158.png

This dependency on the FRO16K is not clearly stated in the reference manuals of the MCXN947 MCU. I will ask the responsible team for clarification of the correct initialization sequence for the the RTCCLKSEL clock selector that is a part of the RTC subsystem. The FRO16K must be enable to access the RTC subsystem register. We will also provide the fix for the MCXN947 MCU in the Clock tool to provide correct initialization code and dependencies in the Clocks model UI.

In the mean time, use the workaround specified above to use 32kHz crystal oscillator clock source as the LP_OSC clock source.

Best Regards,

Marek Neuzil

946 Views
jmullen_condose
Contributor III

Thank you for this solution. This exact issue exists with mcuxpresso and MCXN236 MCU. 

0 Kudos
Reply
2,680 Views
jimmyli
Contributor V

Hello Marek,

       Update a new case:

       When I configure shown as below, iRTC can be initialized and work, but the second is wrong.

       1>iRTC pin for external xtal32k

jimmyli_0-1767585328488.png

 

       2>iRTC clock

jimmyli_1-1767585357845.png

 

       3>iRTC peripheral

jimmyli_2-1767585392048.png

 

       4>Question

            when I using test code shown as below, the second is wrong.

            Hope you can provide some tips to fix this problem.

            Thanks very much.

jimmyli_3-1767585641939.png --test code

 

jimmyli_4-1767585666780.png --debug print

 

Tags (1)
0 Kudos
Reply
2,643 Views
marek_neuzil
NXP Employee
NXP Employee

Hello @jimmyli,

In your last use case, you disabled the FRO16K internal reference oscillator. I am not sure whether the RTC 32kHz external oscillator and the RTCCLKSEL can work properly when the internal reference FRO16K is disabled. I have recommended to enable the FRO16K and the outputs to VBAT and MAIN domains to properly initialize the 32kHz external oscillator. 

I didn't receive the response for the issue of the OSC_32K initialization yet. When the first issue is resolved and the RTC clock source works reliable we can analyze the iRTC functionality (the iRTC issue may by caused by incorrect initialization of the OSC_32K too). I will urge the answer for the first issue. 

Best Regards,

Marek Neuzil

0 Kudos
Reply
2,495 Views
jimmyli
Contributor V

Hi Marek,

      Got it.

      Thanks a lot.

 

      BTW, I found that only enable external 32k crystal, the iRTC can run but the output of second is wrong. But but, when I let the MCU run continuously, iRTC will run accurately later;.

      It is queer to me.

      You can check again.

 

       Thanks again.

0 Kudos
Reply
3,313 Views
jimmyli
Contributor V

Hello Marek,

         Got it.

         Thanks very much.

0 Kudos
Reply
3,406 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @jimmyli ,

Thanks for your post.  I have reproduced your issue. The “RTC0->CTRL |= RTC_CTRL_CLK_SEL_MASK;” generated by Config Tools does have a problem. I will report it to the internal team. Please refer to the workaround below.

1. Comment out the following code in clock_config.c.

Celeste_Liu_0-1765784200089.png

 

2. In hardware_init.c, call the BOARD_InitBootPeripherals(); function declared in peripherals.h. This file contains the RTC-related configurations generated by the Peripherals Config Tools.

Celeste_Liu_1-1765784554328.png

 

3. Modify the main function to test:

Celeste_Liu_3-1765787140126.png

 

4. Test result:

Celeste_Liu_4-1765787214124.png

 

Hope it helps.

BR

Celeste

 

-----------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-----------------------------------------------------------------------------------------------------------------

 

0 Kudos
Reply
3,402 Views
jimmyli
Contributor V

Hi Celeste,

      Thanks very much for your replying.

      But I have a comment that maybe you need to mask the code shown as below, it maybe affect the code function.

 

      Can you help to check again ?

      Thanks very much.

 

jimmyli_0-1765788496602.png

 

0 Kudos
Reply
3,385 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @jimmyli ,

Please refer to Marek's response on this matter. It appears that FRO16K must be enabled, and the outputs to both VBAT and MAIN domains should be enabled. We are awaiting clarification from the internal team and will address this issue accordingly.

Have a nice day.

BR

Celeste

 

0 Kudos
Reply