compiling for freestanding environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

compiling for freestanding environment

3,809 Views
Xeleqt_Ellan
Contributor I

Hi, Im new in NXP products.  I have an issue regarding in compiling freestanding environment, how to solve it. btw im using QN9090 EVKtoolchain problem.pngtoolchain problem.png

Tags (1)
0 Kudos
Reply
5 Replies

2,371 Views
ping1
Contributor V

I have similar issue when i just updated IDE to v24.12, is there any version between v11.8 & v24.12? Does this warnings matters? shall i just ignore it?

Regards!

Ping

0 Kudos
Reply

3,701 Views
gulnur01
Contributor I

could you solve this problem? I have the same issue and I couldn't. I am working on it. Please write me if you solve the problem. 

0 Kudos
Reply

3,650 Views
Alphabert_Liu
NXP Employee
NXP Employee

Hi @gulnur01 @Xeleqt_Ellan ,

I have tried another way to solve this issue, in the project settings, delete -ffreestanding in Other flags in Miscellaneous and it works.

屏幕截图 2024-07-19 103112.png屏幕截图 2024-07-19 103112.png

Best Regard

Liu

0 Kudos
Reply

3,663 Views
Alphabert_Liu
NXP Employee
NXP Employee

Dear @gulnur01 ,

I tried and encountered a similar problem as yours. Later, I found that changing the version of MCUXpresso IDE allowed the project to run normally. You can try changing the version of the IDE.

Best Regard

Liu

0 Kudos
Reply

3,770 Views
Alphabert_Liu
NXP Employee
NXP Employee

Hello @Xeleqt_Ellan ,

Regarding the EVK you are currently using, I recommend that you refer to the official SDK  provided for setting up your project so that you can focus on the core development tasks rather than getting stuck on setting up the environment or encountering compatibility issues.

You can download the SDK through the following link. Select Board | MCUXpresso SDK Builder (nxp.com)

屏幕截图 2024-07-10 154205.png屏幕截图 2024-07-10 154205.png

Search for your hardware and then build SDK.

屏幕截图 2024-07-10 155038.png屏幕截图 2024-07-10 155038.png

Choose your system model, select the IDE: MCUXpresso, and pick the features you need.

屏幕截图 2024-06-26 143215.png屏幕截图 2024-06-26 143215.png

Drag SDK file to the area above, then you can import SDK examples.

Hope my answer may help you.

Best regard, 

Liu

0 Kudos
Reply