Windows ARM64 support request (LinkServer/MCUXpresso)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows ARM64 support request (LinkServer/MCUXpresso)

1,171 Views
VersD
Contributor I

This a request to also start releasing a Windows ARM64 version of LinkServer and the MCUXpresso Installer. I lately see more students using these ARM-based windows laptops.

Labels (3)
0 Kudos
Reply
4 Replies

1,020 Views
VersD
Contributor I

Thank you for the reply. The vscode extension works properly. The mcu-link driver is based on WinUSB which Microsoft ported neatly.  I didn't have admin rights on the test system, but i was able to copy linkserver to the system and debug projects. I don't know about other drivers within the LinkServer installation, but they'd need a signed arm version.

Unfortunately all the tools installed by the "mcuxpresso installer" are x64, so everything runs through the Prism translation layer. git,python,ninja,cmake etc. should have arm versions released already so could be packaged. Only the arm-none-eabi toolchain doesn't have a arm64 version released yet, but could be built. Specifically for mcu-link dev boards it's mostly about performance on the ARM64 windows version.

0 Kudos
Reply

653 Views
luis_maravilla
NXP Employee
NXP Employee

Hi!
Good to hear that it works properly for you, as for an update on the topic, unfortunately we won't be doing this ARM64 for MCUXpresso IDE as we are only doing maintenance on that platform now, the recommendation is still using VS Code extension for MCUXpresso.

Best Regards, Luis

0 Kudos
Reply

609 Views
VersD
Contributor I

The MCUXpresso installer is used by the VSCode extension, which is what I was talking about: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools... and https://mcuxpresso.nxp.com/mcux-vscode/latest/html/MCUXpresso-Installer.html . This is released for macOS x64/arm64 and linux/windows x64 but not arm64. This package includes link server , which is released for macOS x64/arm64 , linux x64/arm64 but for windows x64. My request is for those applications to get released for windows arm64. I understand that the mcuxpresso installer installs a bunch of things, which mostly already are available for windows arm64. I work with students owning these new windows arm64 laptops, now I have to help them with workaround to get things to work.

0 Kudos
Reply

1,136 Views
luis_maravilla
NXP Employee
NXP Employee

Hello,

Thank you for your recommendation, I will comment on this to the correspondent team,

For using MCUXpresso could you help us try using the Visual Studio Code extension? And let us know your findings?

You can read more about the installation and use fort this tool in

MCUXpresso for VS Code documentation — MCUXpresso for VS Code 26.05 documentation

MCUXpresso for Visual Studio Code | NXP Semiconductors

 

Best Regards, Luis

0 Kudos
Reply