Why does the FRDM‑MCXA346 Design Files archive contain a schematic for FRDM‑MCXA166?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why does the FRDM‑MCXA346 Design Files archive contain a schematic for FRDM‑MCXA166?

跳至解决方案
923 次查看
igoreq1010
Junior Contributor IV

Hello,

while reviewing the FRDM‑MCXA346 design files from the NXP download section, I noticed that the included schematic is labeled for FRDM‑MCXA166 instead of FRDM‑MCXA346.

Could you clarify:

  1. Is this intentional and are both boards sharing the same schematic?

  2. Or is this a packaging error in the archive?

  3. Are the MCXA166 and MCXA346 MCUs actually different devices, or is MCXA346 just a newer designation for MCXA166?

I would appreciate if someone from NXP could confirm whether the provided schematic is correct for FRDM‑MCXA346.

I downloaded the archive from the NXP page, and it is named "FRDM‑MCXA346‑DESIGN‑FILES.zip"

 

Thanks in advance!

— Igor

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
580 次查看
Habib_MS
NXP Employee
NXP Employee

Hello @igoreq1010,

The link has been updated, and the design files for the FRDM‑MCXA346 are now available for download.
BR
Habib

在原帖中查看解决方案

2 回复数
581 次查看
Habib_MS
NXP Employee
NXP Employee

Hello @igoreq1010,

The link has been updated, and the design files for the FRDM‑MCXA346 are now available for download.
BR
Habib

838 次查看
Habib_MS
NXP Employee
NXP Employee

Hello @igoreq1010,


Thank you for letting us know. We are working to resolve this issue. I appreciate your patience and will get back to you as soon as we update the link.

BR
Habib.

0 项奖励
回复