Why I am getting problem in pin, clock configuration and debugging for mcxn546v in MCUXpresso IDE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why I am getting problem in pin, clock configuration and debugging for mcxn546v in MCUXpresso IDE?

Jump to solution
3,468 Views
Elakiya
Contributor III

I am beginner in MCUXpresso IDE, I have tried to test my own PCB with MCU MCXN546V and its UART2 pins TX and RX were connected to Neoway N58 IoT board. So I created a fresh project to test the UART protocols and peripherals. But I have received error at debugging given below

[MCUXpresso Semihosting Telnet console for 'MCXN546_Project JLink Debug' started on port 63440 @ 127.0.0.1] SEGGER J-Link GDB Server V8.44 - Terminal output channel.

Later I tried to include SDK for MCXN546V zip file from the dashboard and dragged and dropped, but still I am facing error in added the zip and after adding getting error in clocks, pins configurations. I attached the shreenshot with this post. Please share any example project with MCXN546V pin, clock configurations for uart test.clock_config err.png

Labels (1)
0 Kudos
Reply
1 Solution
3,259 Views
Habib_MS
NXP Employee
NXP Employee

Hello @Elakiya,

This problem seems to be closely related to the communication between the debugger and the core. Most likely, this problem may be due to the software. To address it more effectively, could you please share the full log output from your terminal? This will help me obtain more detailed information and work a more precise solution.

However, since this topic is diverging from the original question, would you mind creating a new community post so we can continue the support there? Feel free to tag me. I will be happy to keep assisting you in the new thread.

BR
Habib

View solution in original post

0 Kudos
Reply
9 Replies
3,438 Views
Habib_MS
NXP Employee
NXP Employee

Hello @Elakiya,

The error occurs because the SDK was generated using the ARMGCC option. This option is intended specifically for use with MCUXpresso IDE for VS Code.

Habib_MS_0-1770850649384.png

If you plan to use MCUXpresso IDE, you must instead choose “Other” and then select MCUXpresso IDE, as shown in the image below:

Habib_MS_1-1770850818061.png

Once you download the correct SDK, simply drag and drop the file into the “Installed SDKs” view inside MCUXpresso IDE to install it.
You can also download SDKs by following the steps mentioned in this post. Even though the example is for the RT1060, the process is exactly the same for the MCXN546.

For help with Config Tools, there is a User Guide available on this page, which may be helpful.

If you have any further questions, do not hesitate to let me know.

BR
Habib

 

 

3,416 Views
Elakiya
Contributor III

Hello, @Habib_MS, Thanks for your response, I have tried to include the proper SDK download for MCUXpresso IDE from the NXP dashboard "other" option. But after freshly reinstalling MCXN546 sdk file, and creating the project, the pin, clock configuration are not opening, I am facing issue with configuration which is shown in screen shot. If anyone have MCXN546V chip SDK for custom PCB chip with MCUXpresso IDE,

Workspace.png

 

please share.547_546_collapse.JPG

0 Kudos
Reply
3,260 Views
Habib_MS
NXP Employee
NXP Employee

Hello @Elakiya,

This problem seems to be closely related to the communication between the debugger and the core. Most likely, this problem may be due to the software. To address it more effectively, could you please share the full log output from your terminal? This will help me obtain more detailed information and work a more precise solution.

However, since this topic is diverging from the original question, would you mind creating a new community post so we can continue the support there? Feel free to tag me. I will be happy to keep assisting you in the new thread.

BR
Habib

0 Kudos
Reply
3,233 Views
Elakiya
Contributor III
Thanks @Habib_MS, you have solved configuration part in my board issue. For debugger issue we will discuss in the new community post. Thanks for your guidence.
3,380 Views
Habib_MS
NXP Employee
NXP Employee

Hello @Elakiya,
The issue is caused by incorrect information stored in SDK package new project template, specifically in the file called "clock_config.c", there is incorrect ID of the package:

Habib_MS_2-1771007733515.png

To work around the issue, in SDK package you downloaded please set package_id as is shown in the file called "pin_mux.c":

Habib_MS_1-1771007687242.png

Making this change I am able to use config tools for MCXN546.

If you experience any issue, do not hesitate to let me know.
BR
Habib.

3,353 Views
Elakiya
Contributor III

Hello @Habib_MS ,  Thanks a lot, after making changes in package_id I can open pin and clock configurations, but after that I tried to flash and debug this project code to my PCB board through segger J-Link, once I start my debugging it stuck inside the file startup_mcxn546_cm33_core0.c as shown in screen shot.  And in console tab I am getting 

[MCUXpresso Semihosting Telnet console for 'MCXN546_Project JLink Debug' started on port 60310 @ 127.0.0.1]

SEGGER J-Link GDB Server V8.44 - Terminal output channel


If I try to pause and resume, it is entering to break page and showing "Break at address "0x20018040" with no debug information available, or outside of program code."

Kindly give solution for this, with example project

debug_stuck.png

Tags (3)
0 Kudos
Reply
3,307 Views
Habib_MS
NXP Employee
NXP Employee

Hello @Elakiya,
Please follow the points mentioned in this post:
MCUXpresso + Jlink - Cannot convert encoding - NXP Community

If the issue persists, do not hesitate to let me know.
BR
Habib

0 Kudos
Reply
3,288 Views
Elakiya
Contributor III

Hello @Habib_MS , Thank you very much for sharing the steps, but even after following the steps, I am getting same issue. Is it any memory issue or PCB power pins issue? I could not identify it. I have shared the screenshot and PCB design circuit diagram png file in this post please check and let me know. Thanks in advance. Screenshot_debug.png

0 Kudos
Reply
3,453 Views
Elakiya
Contributor III

When I try to add MCXN546 SDK zip to MCUXpresso IDE , I get this error, why?  sdk_error.JPG
The added SDK zip file is properly downloaded from the NXP dashboard, but still why this issue?sdk_dwnld.JPG

Please guide to solve this issue

0 Kudos
Reply