Virtualbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Virtualbox

1,844 Views
Peter19
Contributor II

#Linkserver MCUXPRESSO-VSC 

I get problems starting a debug session on win vbox vm.

Anyone tried this?

Labels (2)
0 Kudos
Reply
3 Replies

1,727 Views
Peter19
Contributor II

@Harry_Zhang 

Hello, I’m attempting to debug the FRDM‑MCXN947 board using the MCUXpresso VS Code extension (v25.11.16) with LinkServer as the debug probe.

My environment is:

  • Host OS: Windows 11

  • Guest OS: Windows 11 (VirtualBox VM)

  • MCUXpresso VS Code extension: 25.11.16

  • Debug probe: LinkServer

  • Target board: FRDM‑MCXN947

Problem: When I start a debug session inside the VM, the session fails to launch. The extension is installed correctly, but the debugger does not connect to the target.

Question: Has anyone successfully run LinkServer debugging in this configuration (Windows 11 host + Windows 11 guest in VirtualBox)? Are there known limitations or required configuration steps for USB passthrough or driver setup in VirtualBox that affect LinkServer?

Thanks for any guidance.

0 Kudos
Reply

1,659 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Peter19 

LinkServer requires low-level USB/HID access, but VirtualBox USB passthrough is unstable for HID-class debug probes.

So i think LinkServer debugging rarely works reliably inside VirtualBox.

I think you can try to  Debug on the HOST, not the VB
you can use MCUXpresso IDE on Host or MCUXpresso VS Code extension on Host.

BR

Harry

0 Kudos
Reply

1,811 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Peter19 

Can you describe your issue in detail?

BR

Harry

0 Kudos
Reply