VScode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VScode

2,101 Views
damonyun
Contributor I
 

 

使用VScoode开发的时候,导入工程后,编译提示生成的board_files.cmake有错误,里面只有endif. Snipaste_2026-04-08_11-40-22.png

Labels (1)
0 Kudos
Reply
5 Replies

2,079 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @damonyun 

请问您是使用什么版本的MCXN947 SDK?

 

Snipaste_2026-04-08_15-36-04.png

请问您MCUXpresso installer 中的MCUXpresso SDK Developer 是否安装成功?

BR

Harry

0 Kudos
Reply

2,063 Views
damonyun
Contributor I
SDK版本是26.3
0 Kudos
Reply

2,064 Views
damonyun
Contributor I

安装了,检查也通过的

Snipaste_2026-04-08_16-27-26.png

0 Kudos
Reply

2,054 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @damonyun 

我刚刚在我这边测试了SDK_26_03_00_FRDM-MCXN947。可以编译成功。

下面是我的步骤,

1. 下载SDK_26_03_00_FRDM-MCXN947 sdk 包。

MCUXpresso SDK Builder

Snipaste_2026-04-08_17-58-57.png

2.  导入下载的sdk包到MCUXpresso for vscode 中。

Snipaste_2026-04-08_18-00-47.png

 3. 从repo中导入helloworld demo

Snipaste_2026-04-08_18-01-26.png

 

4 编译  

Snipaste_2026-04-08_18-02-50.png

 请问您的测试步骤跟我的一样么?

BR

Harry

0 Kudos
Reply

2,023 Views
damonyun
Contributor I

在此之前,安装工具和sdk包后我都只尝试了Freestanding application,一直失败。

根据你的流程,尝试了repo之后,工具看起来一切都正常了!

非常感谢您的回复,后续出现问题我再重新提交。

image.png

0 Kudos
Reply