Using dma to update gpio->ptor register does not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using dma to update gpio->ptor register does not work

691件の閲覧回数
Vipul_Shukla
Contributor I

I am trying to configure dma to toggle gpio pin using ptor register for that gpio but even after the dma transfer is done the pin is not toggled. DMA is trig match events. I am using frdmmcxn947 board. 

If I am trying to transfer to a local buffer then the transfer is working as expected but if I change the destination address to GPIO2->PTOR register or even PDOR register then it is not working.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

686件の閲覧回数
Vipul_Shukla
Contributor I

I have attached my project zip file

 

0 件の賞賛
返信

428件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Vipul_Shukla 

I checked your code.

    EDMA_PrepareTransferConfig(&transferConfig1, &data, 4, 0, (void*)&GPIO2->PDOR, 4, 0, 4, 4);

You used the PDOR register.

You can check the GPIO_PortToggle.

Harry_Zhang_0-1745381102771.png

It use PTOR, not PDOR.

So you should change it to PTOR.

BR

Harry

0 件の賞賛
返信