USB composite device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB composite device

1,846 次查看
allu
Contributor I

HI NXP,

We are developing a USB compostie device based on the NXP SDK_2_14_0_FRDM-MCXN236_rfp USB device example, with an MCTP class (using endpoints 1 and 2) and an HID class (using endpoints 3 and 4).

I modified the following:

#define USB_DEVICE_CONFIG_ENDPOINTS (5U)

I found that only endpoints 1 and 2 work—the MCTP class functions correctly, but the HID class does not.

However, when I change it to use the MCTP class on endpoints 3 and 4 and the HID class on endpoints 1 and 2, the HID class works, but the MCTP class does not.

 

Could you tell me if the endpoint settings need to be modified?

 

Thanks,

Alan

 

 

标签 (1)
0 项奖励
回复
1 回复

1,795 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @allu

There is a composite demo available in the SDK that also uses 5 endpoints. You might find it helpful to refer to this demo for configuration guidance.

Alice_Yang_0-1730359308900.png

 

BR

Alice

 

 

0 项奖励
回复