Trouble getting NXPNCI Library to work with an MCXN236 MCU and OM27160A1EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trouble getting NXPNCI Library to work with an MCXN236 MCU and OM27160A1EVK

ソリューションへジャンプ
3,044件の閲覧回数
shalom_greene
Contributor III

I've ported the NXPNCI library examples over to a MCXN236 MCUXpresso board and keep getting errors within the NxpNci_CheckDevPres() function. It seems to fail on sending the NCICoreReset data. I've confirmed correct HW connections, but continue to get data failures in 3 different scenarios:

Scenario #1: Using FLEXIO_I2C_MasterTransferBlocking() with no retries, the program hangs in an infinite loop after receiving a shifter error flag from the FLEXIO module (which is interpreted as a NACK).

Scenario #2: Using FLEXIO_I2C_MasterTransferBlocking() with retries (3), the program aborts the write process after receiving a shifter error flag from the FLEXIO module (which is interpreted as a NACK).

Scenario #3: Using FLEXIO_I2C_MasterTransferNonBlocking() with retries (3), the program writes with no error, but fails when attempting to receive an answer back from the PN7160 NFC chip. This results in continuous writes with no returned data.

 

Per https://www.nxp.com/docs/en/user-manual/UM11496.pdf, I am setting up the pins accordingly and using the default device address 0x28. 

I'm currently using the FLEXIO_I2C functions in place of the I2C functions called out in the original TML files for the examples. Since I'm using the pin, clock and peripheral configuration tools, I had to reroute some of the code in the TML files to point to the pin_mux.h/.c and peripheral.h/.c files.

 

I've attached the project here if anyone has the HW and wants to try. NOTE: because of file size limits, I had to separately compress the debug folder outside of the project folder. To bring up this project, you will either have to decompress the debug folder and place it  back into the root folder for the project - OR - create a new debug as MCUXpresso IDE LinkServer.

 

Pinout from MCXN236 to OM27160 are as follows...

SCL: FLEXIO D21 (J4, Pin 12) ---> J2, Pin 1

SDA: FLEXIO D20 (J4, Pin 10) ---> J2, Pin 2

GND: J4, Pin 3 ---> J1, Pin 6

VDD: 3.3V (J3, Pin ---> J1, Pin 4

VBAT: 5V (J3, Pin 10) ---> J1, Pin 5

IRQ: J7, Pin 4 ---> J1, Pin 10

VEN: J7, Pin 5 ---> J4, Pin 1

DWL_REQ: J6, Pin 6 ---> J4, Pin 2

0 件の賞賛
返信
1 解決策
2,759件の閲覧回数
shalom_greene
Contributor III

I was finally able to get this pairing to work. A clue that helped me was getting the LPC824 example working, which didn't work unless I had the board directly mounted on top (no extra cable length attached between boards), which seems like a drive strength issue for the MCUXpresso boards.

 

Understanding that, I reconfigure my MCXN Xpresso board to have the same pinout that aligns with the arduino headers that connect to the OM27160A1EVK. Once I did that, I placed the OM27160A1EVK board directly on top of the Xpresso board using J1 through J4. I then, just soldered pins on top of the OM27160A1EVK I2C and IRQ signals to probe with a logic analyzer.

 

Image20250313170527.jpg

 

Another caveat that I noticed is that the program only seems to work when debug output (NCI_DEBUG) is enabled. For some reason, a time delay is needed between a buffer read and when it is being accessed for comparison. Otherwise, I get failures when the NCI library is comparing the received data to the expected response bytes. My assumption is that the debug adds extra time between read/write and buffer access, allowing the buffer to make the correct data available in memory.

 

The specific design that I'm working on should be tolerant of a small delay in reads, but this seems like a flaw for the MCXN236.

 

元の投稿で解決策を見る

0 件の賞賛
返信
12 返答(返信)
2,760件の閲覧回数
shalom_greene
Contributor III

I was finally able to get this pairing to work. A clue that helped me was getting the LPC824 example working, which didn't work unless I had the board directly mounted on top (no extra cable length attached between boards), which seems like a drive strength issue for the MCUXpresso boards.

 

Understanding that, I reconfigure my MCXN Xpresso board to have the same pinout that aligns with the arduino headers that connect to the OM27160A1EVK. Once I did that, I placed the OM27160A1EVK board directly on top of the Xpresso board using J1 through J4. I then, just soldered pins on top of the OM27160A1EVK I2C and IRQ signals to probe with a logic analyzer.

 

Image20250313170527.jpg

 

Another caveat that I noticed is that the program only seems to work when debug output (NCI_DEBUG) is enabled. For some reason, a time delay is needed between a buffer read and when it is being accessed for comparison. Otherwise, I get failures when the NCI library is comparing the received data to the expected response bytes. My assumption is that the debug adds extra time between read/write and buffer access, allowing the buffer to make the correct data available in memory.

 

The specific design that I'm working on should be tolerant of a small delay in reads, but this seems like a flaw for the MCXN236.

 

0 件の賞賛
返信
2,860件の閲覧回数
shalom_greene
Contributor III

Hello @KaiLi,

 

I momentarily switched over to one of the recommended platforms (LPC824) to see how it's expected to work and I've run into a couple of issues...

  1. Sometimes the program fails on the last command before discovery.
  2. On successful start of discovery, the device goes into an infinite loop inside of NxpNci_WaitForDiscoveryNotification() and never drops into the polling loop for card type.

 

Please see attached debug log.

0 件の賞賛
返信
2,822件の閲覧回数
shalom_greene
Contributor III

@KaiLi ,

 

In the case when it starts discovery and then enters an infinity loop, I see that the SCL and SDA lines get out of sync and there is a repeated pattern of read 0x7F with NACK

 

shalom_greene_0-1741880005499.png

This screenshot above shows the bursts of data that occurs in the infinite loop in ~500ms intervals.

 

shalom_greene_3-1741880419399.png

This screenshot above shows the repeated ~15ms burst of data that occurs every ~500ms.

 

shalom_greene_2-1741880188686.png

Screenshot above shows the data within that burst in a zoomed in view. It also shows SDA and SCL getting out of sync and the IRQ signal toggling.

 

0 件の賞賛
返信
2,828件の閲覧回数
shalom_greene
Contributor III

@KaiLi ,

 

Is there a list of commands that I can view to help debug? Sometimes I get an unexpected response. The NCIStartDiscovery command in NxpNci_StartDiscovery() is expecting [0x41, 0x03] for the first two byte, but gets back [0x41, 0x00]. Currently, I have no way of telling what this is supposed to mean.

 

Running the NXP-NCI2.0 example.
NCI >> 20 00 01 01
NCI << 40 00 01 00
NCI << 60 00 09 02 01 20 04 04 71 12 50 05
NCI >> 20 01 02 00 00
NCI << 40 01 1e 00 1a 7e 06 03 01 d0 02 ff ff 01 ff 00 08 00 00 01 00 02 00 03 00 80 00 82 00 83 ...
NCI >> 2f 00 01 00
NCI << 4f 00 01 00
NCI >> 20 02 05 01 00 02 fe 01
NCI << 40 02 02 00 00
NCI >> 20 03 03 01 a0 14
NCI << 40 03 25 00 01 a0 14 20 57 65 64 20 4d 61 72 20 31 32 20 31 34 3a 33 30 3a 30 35 20 32 30 ...
NCI >> 20 00 01 00
NCI << 40 00 01 00
NCI << 60 00 09 02 00 20 04 04 71 12 50 05
NCI >> 20 01 02 00 00
NCI << 40 01 1e 00 1a 7e 06 03 01 d0 02 ff ff 01 ff 00 08 00 00 01 00 02 00 03 00 80 00 82 00 83 ...
NCI >> 2f 02 00
NCI << 4f 02 05 00 00 01 aa dd
NCI >> 21 00 10 05 01 01 01 02 01 01 03 01 01 04 01 02 80 01 80
NCI << 41 00 01 00
NCI >> 21 03 07 03 00 01 01 01 06 01
NCI << 41 00 01 00 00 01 aa dd 01 d0
Error: cannot start discovery

0 件の賞賛
返信
2,857件の閲覧回数
shalom_greene
Contributor III
More context on the hang up: The program seems to get hung up in NxpNci_WaitForReception() function. I suppose this is due to not acknowledging the NFC tag. I've tried reading from multiple type 2 and type 5 tags and none seem to be recognized. Is this reader only compatible with specifically formatted tags?
0 件の賞賛
返信
3,009件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @shalom_greene 

The problem should be in the porting of I2C driver , so you need to check whether the I2C communication is correct between MCU and PN7160. 

Also, you can refer to the section 12.1 of AN13892 (https://www.nxp.com.cn/docs/en/application-note/AN13892.pdf) and trigger the NCI log to see what happened on your side. 

0 件の賞賛
返信
2,941件の閲覧回数
shalom_greene
Contributor III

@KaiLi,

 

Thanks for sharing the expected data from the example. I was able to modify the TML file enough to confirm the results of the NxpNci_CheckDevPres() function. I seem to get that data back fine, but then fail on the next command of NxpNci_HostTransceive(). It returns with no data. Initially, I thought that I needed a longer wait period for the data to be ready and IRQ to generate, but the IRQ signal remains low indefinitely after sending the NCICoreInit_2_0 (0x20, 0x01, 0x02, 0x00, 0x00) command.

 

Also, sometimes I notice that the data seems buffered or delayed from the PN7160. This seems to occur when the system comes up with the IRQ already high. I expect that the reset toggle on the VEN pin should set the IRQ back low, but it doesn't always do so. 

 

Here is the data transaction that I'm getting.

Screenshot 2025-03-10 170330.png

Screenshot 2025-03-10 172049.png

I have to note here that I had to modify the tml_Receive() function to get this to work this far. And the system still only seems to work when using non-blocking I2C transfer functions.

 

Here's the code snippet for the receive function that I modified:

void tml_Receive(uint8_t *pBuffer, uint16_t BufferLen, uint16_t *pBytes, uint16_t timeout) {

PRINTF("\n\r*** New Read Triggered! ***\n\r");

 

//clear out buffer

memset(pBuffer,0x00,BufferLen*sizeof(uint8_t));

//Sleep(300);

tml_WaitForRx(timeout*10); //currently discarding error

Status ret = tml_Rx(pBuffer, BufferLen, pBytes);

 

PRINTF("\n\rtml_Rx status: %i, buffer length: %i\n\r", ret, *pBytes);

PRINT_BUF("\n\r***Current Buffer Content: ", pBuffer, *pBytes);

 

if ((GPIO_PinRead(BOARD_NXPNCI_IRQ_GPIO, BOARD_NXPNCI_IRQ_PIN) == 1)) {

PRINTF("\n\r*** IRQ still asserted! More data to read... ***\n\r");

PRINT_BUF("\n\r**BEFORE RETRY*** NCI << ", pBuffer, *pBytes);

if (ret == SUCCESS) {

PRINTF("\n\r*** Attempting to read remaining data. ***\n\r");

if(INTF_READ(&pBuffer[*pBytes], pBuffer[2]) == kStatus_Success)

{

*pBytes = *pBytes + ((pBuffer[2] + 3) - *pBytes);

}

else

{

PRINTF("\n\r*** Failed to read additional bytes ***\n\r");

}

}

else {

PRINTF("\n\r*** tml_Rx Failed initial read. Attempting to retry read with INTF_READ. ***\n\r");

if(INTF_READ(&pBuffer[*pBytes], pBuffer[2]) == kStatus_Success)

{

*pBytes = pBuffer[2] + 3;

}

else

{

PRINTF("\n\r*** Failed to read additional bytes ***\n\r");

}

}

PRINT_BUF("**AFTER RETRY*** NCI << ", pBuffer, *pBytes);

}

 

PRINTF("\n\rtml_Rx status: %i, buffer length: %i\n\r", ret, *pBytes);

PRINT_BUF("\n\r***Current Buffer Content: ", pBuffer, *pBytes);

}

 

Please also see log attached with some debug output.

0 件の賞賛
返信
2,937件の閲覧回数
shalom_greene
Contributor III

Here's an updated, formatted image of the code snippet.

 

Screenshot 2025-03-10 172702.png

0 件の賞賛
返信
2,988件の閲覧回数
shalom_greene
Contributor III

Hello @KaiLi,

 

Thanks for the quick reply. I understand that there is an issue with the I2C communication. I just can't figure out what exactly is wrong. I've switch from using FLEXIO_I2C to use LPI2C via LP_Flexcomm, but I get the same results. When using the blocking transfer function, transmission aborts due to shifter error status flags. When using nonblocking transfer functions, I can see the data being transmitted out, but I get no reply form the PN7160.

 

I see that the data being transmitted is being acknowledged by the PN7160 device, but I'm not getting a response when trying to receive. The User Manual documentation for PN7160 says to wait for the IRQ pin to go high before requesting data. I see it go high, but it's in the middle of the data transfer. There is a function tml_Rx() in the NXPNCI Library that waits for this pin to go high but fails due to timeout. The pin only remains high for about 160ns, and seems to coincide with a glitch in the clock signal. So, the function aborts before attempting to read due to missing the interrupt. This occurs while sending the NCICoreReset command. Is this command expected to return any data?

Also, I assume that the fact that I'm getting ACKs back from the PN7160 means that it's alive, but how do I confirm that it's not in standby mode? I read that if the device is in standby mode, it will not respond

Here is the data that I've captured on a logic analyzer using the non-blocking transfer functions:

 

Screenshot 2025-03-07 125133.png

 

Screenshot 2025-03-07 151026.png

 

 

 

0 件の賞賛
返信
2,977件の閲覧回数
shalom_greene
Contributor III

I realized that I didn't have the logic analyzer grounded. So, once I sync'd the grounds, I no longer see the glitch. So, I'm back to seeing data transmitted with ACK on each byte, but no IRQ or data generated by the PN7160.

So, my question still stands on how to ensure that the PN7160 is not in standby mode.

Feedback on the OM27160 devkit: It would be nice to have some LEDs to know status of the HW (i.e. RX/TX data being received/sent and an indicator for standby vs active mode). Right now, there is no way to tell what mode it's in and the WUP_REQ pin that is suggested for forcing the PN7160 out of standby is a NC according to the schematics.

 

Screenshot 2025-03-07 170427_1.png

0 件の賞賛
返信
2,889件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @shalom_greene 

If you want to make sure the PN7160 is not in standby mode, you can configure it as follows:

/* NXP-NCI standby enable setting
* Refer to NFC controller User Manual for more details
*/
uint8_t NxpNci_CORE_STANDBY[]={0x2F, 0x00, 0x01, 0x00}; /* last byte indicates enable/disable */

0 件の賞賛
返信
2,886件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @shalom_greene 

uint8_t NxpNci_CORE_STANDBY[]={0x2F, 0x00, 0x01, 0x00}; /* last byte indicates enable/disable */

0x00: disable Standby

0x01: enable standby

0 件の賞賛
返信