The start signal is not responding of PT2001

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The start signal is not responding of PT2001

1,044 次查看
richer
Contributor I

We designed the circuit using the recommended circuit diagram from PT2001 and generated microcode using the default code from PT2001Dev studio. The current problem is that the BOOST voltage can be boosted to 65V normally, but after driving the DRVEN and START signals, the fuel injector has no response. How can I troubleshoot this situation?

标签 (1)
0 项奖励
回复
2 回复数

1,016 次查看
richer
Contributor I

Hi LexLiu,

Thank you for your help. Due to our special engineering requirements, we may need to connect 1, 2, 3, or 4 fuel injectors in actual use. My current demo only connects 1 and 2 fuel injectors. During the self-test process, the Bootstrap check's rxData=send_stngle_SPI_Cmd (READ, ioobuttostrap_charged, 0x00); I read 0xD394, and this self-test failed, so I annotated this check. May I ask if this is related to the fact that the startup signal is not working after me? Additionally, how can I configure an application that meets my requirement for connecting the number of fuel injectors freely?

0 项奖励
回复

1,027 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Lex (@LexLiu),

Could you please help with this question regarding the PT2001 from Beijing Yi'an Hengrui Technology?

Thanks & BRs, Tomas

0 项奖励
回复