TJA1152 Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1152 Configuration

2,492件の閲覧回数
stevenlutz
Contributor III

Where can I find the documentation on the TJA1152?
I'm using the MCXN947 flexcan interrupt transfer demo but need to whitelist CAN ID 0xDF80502 as well as others preferably with a mask?
or maybe disable security features all together on TJA1152.

Some direction on how this is done would be really helpful. Even if it's just the guide on the TJA1152 commands and configuration. 


ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,478件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @stevenlutz ,

Thanks for your post.

Please refer to the product page of TJA1152 on the NXP official website: TJA1152 Secure HS-CAN Transceiver | NXP Semiconductors
There are several documents related to TJA1152 available on this page.

Celeste_Liu_0-1737458847556.png

And you can also refer to the Secure CAN Demo Using TJA115x Transceivers | NXP Semiconductors.

Hope it can help you.

BRs,

Celeste

---------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------------------------

 

 

0 件の賞賛
返信

2,460件の閲覧回数
stevenlutz
Contributor III

None of those documents available are the reference manual that I was looking for. However, I have realized that the tja1152, while supported in the can demo, isn't actually used, which is now taking me back to the unresponded post / issue here

https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-CanBus-Rx-Stop-Receiving/m-p/2030106#M2371

 

Please help. Thank you. 

タグ(1)
0 件の賞賛
返信

2,463件の閲覧回数
stevenlutz
Contributor III

None of those documents available are the reference manual that I was looking for. However, I have realized that the tja1152, while supported in the can demo, isn't actually used, which is now taking me back to the unresponded post / issue here

https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947-CanBus-Rx-Stop-Receiving/m-p/2030106#M2371

 

Please help. Thank you. 

0 件の賞賛
返信

2,434件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @stevenlutz ,

Thank you for your feedback. I've noticed that the post you mentioned is being handled by my colleague. It seems that the issue in this post has been resolved. I will close this thread for now. If you have any new questions, feel free to create a new post.

BRs,

Celeste

0 件の賞賛
返信