Smallest (and cheapest) MCX part/package for USB Audio?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Smallest (and cheapest) MCX part/package for USB Audio?

988 次查看
dav1
Contributor V

Hi,

Since there are now many families within the MCX series, I'd like some guidance to narrow down

  • which part-no's can run usb-audio
  • small footprints <5x5mm
  • lowest cost / minimal peripheral-set 

 

A good match would be HS-usb, 4x4mm package still 0.5mm pitch. one I2S. a few gpio's, price <$1.0/pcs

标签 (4)
0 项奖励
回复
3 回复数

913 次查看
dav1
Contributor V

thanks alice,

I also looked at the LFBGA64 parts which are also 5x5mm

• MCXC443VMP (only 16K ram, so might be too little for the stack)
• MCXC444VMP (32K, and also 256K flash meaning slightly higher prise point)

another alternative might be the 
• LPC5514JEV59 series (59BGA = 4x4mm), higher price probably due to more memory

905 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @dav1 

Yes, you can choose from these chips. Thank you.

BR

Alice

0 项奖励
回复

941 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @dav1 

I recommend two products to you.

One is the MCXC243VFT. It mostly meets all your requirements, except for the body size. Its size is 7mm*7mm. For details, please refer to: https://www.nxp.com/part/MCXC243VFT.

Another one is the MCXC244VFM. The only requirement it doesn't meet is the price. The budgetary price is $1.05 USD for 10,000 pieces, and its features all meet your requirements. For details, please refer to: https://www.nxp.com/part/MCXC244VFM.

Both of the two products support Full-speed USB, not HS-speed. 

BR

Alice

0 项奖励
回复