SDRAM connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM connection

1,888件の閲覧回数
Hessam_Shafaghi
Contributor I

Hi,

I want to use an SDRAM (64Mb Synchronous Dynamic RAM) in my design based on MCXN23x. I couldn't find any information or a sample circuit diagram about it. I found out that only there is a way to connect it using FLEXIO; but I'm unsure. 

Does anybody have any idea or similar experience?

Thanks

タグ(1)
0 件の賞賛
返信
1 返信

1,859件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello, I hope you are well. 

FlexIO can emulate different parallel interfaces however it will be difficult to integrate parallel SDRAM as FlexIO only has 32 pins. 

One alternative to this is using a serial RAM so you can emulate the interface on FlexIO: Using FlexIO to emulate Quad SPI master (nxp.com)

Best regards,
Omar