Request for Assistance: Troubleshooting SPI Configuration for Qualcomm QCA7005 PLC Module on i.MX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Assistance: Troubleshooting SPI Configuration for Qualcomm QCA7005 PLC Module on i.MX8MP

2,323 Views
yongha_yu
Contributor II
I'm encountering difficulties getting my PLC module, utilizing the Qualcomm QCA7005, to function properly when connected to the ecspi2 interface on the i.MX8MP. Below is the configuration I'm using. Could you please review it for any potential misconfigurations?

&ecspi2 {
        #address-cells = <1>;
        #size-cells = <0>;
        fsl,spi-num-chipselects = <1>;
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_ecspi2>;
        status = "okay";

        qca7000: qca7000@0 {
                status = "okay";
                compatible = "qca,qca7000";
                reg = <0x0>;                                            /* CE0 */
                pinctrl-names = "default";
                interrupt-parent = <&gpio5>;
                interrupts = <3 IRQ_TYPE_EDGE_RISING>;
                spi-max-frequency = <8000000>;
                spi-cpha;                                                       /* SPI mode: CPHA=1 */
                spi-cpol;                                                       /* SPI mode: CPOL=1 */
        };
};

pinctrl_ecspi2: ecspi2grp {
        fsl,pins = <
                MX8MP_IOMUXC_ECSPI2_SCLK__ECSPI2_SCLK           0x82
                MX8MP_IOMUXC_ECSPI2_MOSI__ECSPI2_MOSI           0x82
                MX8MP_IOMUXC_ECSPI2_MISO__ECSPI2_MISO           0x82
                MX8MP_IOMUXC_ECSPI2_SS0__ECSPI2_SS0             0x82
                MX8MP_IOMUXC_SPDIF_TX__GPIO5_IO03               0x144
        >;
};

For context, when connecting the same PLC module to the phyBOARD®-AM62x Development Kit using the TI AM62X, it operates correctly. Any insights you could provide would be greatly appreciated.


0 Kudos
Reply
1 Reply

2,287 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @yongha_yu 

You can refer the imx8mp-evk.dts file for your ecspi device configuration.

B.R

0 Kudos
Reply