Replacing NXP RT1166 to RT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Replacing NXP RT1166 to RT1064

865 Views
OliveiraKOL
Contributor I

I´m using RT1166 on my project, but, one of requirement is the chip should have Internal Flash accessible by JTAG/SWD.  The RT1166 dosnt have, but RT1064 has 4MBytes of internal flash.

 

Can I store and retrieve data on it flash using JTAG/SWD?

Labels (1)
0 Kudos
Reply
1 Reply

848 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @OliveiraKOL ,

 

Yes, it is possible, but you need to have some flash driver running in the RAM to assistant the JTAG access. 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply